AXIS#.HWEN.STATE
Description
This parameter returns the state of the hardware enable input.
If AXIS#.HWEN.SOURCE=0, indicating that no hardware enable input is configured, AXIS.HWEN.STATE always returns 1.
Usage
0: Hardware enable input is low preventing the axis from being enabled.
1: Hardware enable input is high allowing the axis to be enabled.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000# |
General Information
Type | Read Only |
Units | N/A |
Range | 0 to 1 |
Default Value | N/A |
Data Type | Integer |
See Also | AXIS#.HWEN.SOURCE, AXIS#.HWEN.MODE |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
AXIS1.HWEN.STATE |
5009h |
03h |
Unsigned8 |
- |
- |
Read only |
No |
AXIS2.HWEN.STATE |
5109h |
03h |
Unsigned8 |
- |
- |
Read only |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.HWEN.STATE |
7002 |
1B5A |
Unsigned8 |
Read Only |
- |
AXIS2.HWEN.STATE |
72538 |
11B5 |
Unsigned8 |
Read Only |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.HWEN.STATE |
7002 |
Unsigned8 |
Read Only |
- |