AXIS#.IL.IUFB

Description

This parameter displays the measured current in the u-winding of the AXIS#.MOTOR.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

A

Range

± Drive peak current (IPEAK)

Default Value

N/A

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

Current Loop