AXIS#.VL.AINSOURCE
Description
This parameter sets which analog input to use for AXIS#.VL.AINSCALE.
Value | Description |
---|---|
0 | Uses no analog input. The velocity command in analog velocity mode is 0. |
1 | Uses AIN1 |
2 | Uses AIN2 |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
Added '0' to range | 02-07-02-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 2 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
AXIS1.VL.AINSOURCE |
5011h |
20h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.VL.AINSOURCE |
5111h |
20h |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.VL.AINSOURCE |
6040 |
1798 |
Unsigned8 |
Read/Write |
- |
AXIS2.VL.AINSOURCE |
71576 |
1179 |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.VL.AINSOURCE |
6040 |
Unsigned8 |
Read/Write |
- |