DOUT#.SOURCE

Description

DOUT#.SOURCE sets the digital output source.

Value Description
0 - User User controls the output value using DOUT#.STATEU
1 - Action Table Action table controls the output value
2 - FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Fieldbus controls the output value
4 - Compare Compare channel controls the output value

Examples

Usage

0: User controlled. DOUT#.STATE is set by DOUT#.STATEU.

1: Action table controlled. DOUT#.STATE is set by the assigned action, if any.

2: Fieldbus controlled. DOUT#.STATE is set by the fieldbus output control 3601h Digital output control sub 1.

4: Compare channel controlled. DOUT#.STATE is set by the compare channel output. The specific channel is selected by DOUT#.SOURCEID.

Code

The following commands set the source for digital output 1 to user control, and the source for digital output 2 to action table. The user is able to control the state of digital output 1, but not digital output 2.

--> DOUT1.SOURCE 0
--> DOUT1.STATE 0
--> DOUT1.STATEU 1
--> DOUT1.STATE 1
--> DOUT2.SOURCE 1
--> DOUT2.STATE 0

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

 

Added fieldbus source 02-00-01-000  
Add Sequencer source 02-02-03-000  
Added Compare source 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 0, 1, 2, 4
Default Value 0
Data Type Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

DOUT1.SOURCE

360ah

01h

Unsigned8

-

-

Read/Write

No

DOUT2.SOURCE

360bh

01h

Unsigned8

-

-

Read/Write

No

DOUT3.SOURCE

360ch

01h

Unsigned8

-

-

Read/Write

No

DOUT4.SOURCE

360dh

01h

Unsigned8

-

-

Read/Write

No

DOUT5.SOURCE

360eh

01h

Unsigned8

-

-

Read/Write

No

DOUT6.SOURCE

360fh

01h

Unsigned8

-

-

Read/Write

No

DOUT7.SOURCE

3610h

01h

Unsigned8

-

-

Read/Write

No

DOUT8.SOURCE

3611h

01h

Unsigned8

-

-

Read/Write

No

DOUT9.SOURCE

3612h

01h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DOUT1.SOURCE

21150

529E

Unsigned8

Read/Write

-

DOUT2.SOURCE

21151

529F

Unsigned8

Read/Write

-

DOUT3.SOURCE

21152

52A0

Unsigned8

Read/Write

-

DOUT4.SOURCE

21153

52A1

Unsigned8

Read/Write

-

DOUT5.SOURCE

21154

52A2

Unsigned8

Read/Write

-

DOUT6.SOURCE

21155

52A3

Unsigned8

Read/Write

-

DOUT7.SOURCE

21156

52A4

Unsigned8

Read/Write

-

DOUT8.SOURCE

21157

52A5

Unsigned8

Read/Write

-

DOUT9.SOURCE

21158

52A6

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DOUT1.SOURCE

21150

Unsigned8

Read/Write

-

DOUT2.SOURCE

21151

Unsigned8

Read/Write

-

DOUT3.SOURCE

21152

Unsigned8

Read/Write

-

DOUT4.SOURCE

21153

Unsigned8

Read/Write

-

DOUT5.SOURCE

21154

Unsigned8

Read/Write

-

DOUT6.SOURCE

21155

Unsigned8

Read/Write

-

DOUT7.SOURCE

21156

Unsigned8

Read/Write

-

DOUT8.SOURCE

21157

Unsigned8

Read/Write

-

DOUT9.SOURCE

21158

Unsigned8

Read/Write

-