AIN.VALUE
Description
AIN.VALUE reads the analog input value after the value is filtered (as shown in the Analog Input Block Diagram).
General Information
|
Type |
R/O Parameter |
|
Units |
V |
|
Range |
-12.5 to +12.5 V |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNet
SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
| Index/Subindex | Object Start Version |
|---|---|
|
3470h/4 3509h/0 |
M_01-00-00-000 |