AIN.ZERO
Description
AIN.ZERO causes the drive to zero the analog input signal (AIN.VALUE ). You may need to execute this command more than once to achieve zero offset, and AIN.OFFSET is modified in this process.
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Variants Supported
*In SynqNet
SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
*For PROFINET, write a value of 0 into the PNU to execute a command.