IL.KP
Description
IL
"Instruction List"
This is a low-level language and resembles assembly.KP is used to modify the proportional gain of the PI-loop that controls the q-component of the current.
General Information
|
Type |
NV Parameter |
|
Units |
V/A |
|
Range |
0 to 2,000 V/A |
|
Default Value |
Read from the motor or, if no memory, 50.009 V/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Related Topics