MOTOR.IDMAX

Description

This parameter is supported for IPM motors (MOTOR.TYPE = 6). MOTOR.IDMAX is the maximum motor winding current in the direct (non-torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing) axis.


  • This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.

General Information

Type

NV Parameter

Units

Arms

Range

0.2 to 1000

Default Value

0.5 * MOTOR.IPEAK

Data Type

Float

Start Version

M_01-11-00-000

(missing or bad snippet)

Related Topics

Motor View | MOTOR.IPEAK