MOTOR.LDLL

Description

This parameter is the motor line to line direct axis inductance. It is supported for the IPM motor type (MOTOR.TYPE = 6).


  • This parameter is automatically configured for Kollmorgen motors when MOTOR.AUTOSET = 1.

General Information

Type

NV Parameter

Units

mH

Range

1 to 2^31

Default Value

17.000

Data Type

Float

Start Version

M_01-11-00-000

(missing or bad snippet)

Related Topics

Motor View | MOTOR.LQLL | IL.KPDRATIO