MCFB_AKDFaultLookup
Function Block - String message of the corresponding AKD drive fault number.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
BOOL |
0, 1 |
N/A |
No default |
Enables the KollmorgenUDFB. Used in the FFLD editor only. |
|
FaultNumber |
DINT |
No range |
N/A |
No default |
The AKD drive fault number. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
0, 1 |
N/A |
TRUE if there is a match for the FaultNumber. |
|
FaultDescription |
STRING |
N/A |
N/A |
Description of the fault. |
Remarks
- This function or function block can be used with PLCopen Motion engines.
- The FaultNumber is the same number as reported on the display of the AKD drive.
- OK output turns TRUE when the there is a match for the FaultNumber.
- The FaultDescription displays the corresponding text string.
This image shows the function or function block I/O.
Figure 1: MCFB_AKDFaultLookup
Usage
- Provide drive fault information the application program uses to determine next steps.
- Example: Perform a machine-controlled stop or perform an immediate disable of the servo drives.
- In the application program, sends output fault information from this UDFB to the HMI for review by the machine operator.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Execute and Read the Function Block
Inst_MCFB_AKDFault( Axis1(*lib:AXIS_REF*) );
FaultDrive1 := Inst_MCFB_AKDFault.FAULT;
FaultDrive1Number := Inst_MCFB_AKDFault.FaultNumber;
FaultDrive1Description := MCFB_AKDFaultLookup( FaultDrive1Number(*DINT*) );
See Also
- FB_AKDFltRpt
- MC_ReadStatus (PLCopen Motion Engine)
- MCFB_AKDFault