Adder

Name

Description

MLAddInit

Initializes an Adder Pipe Block for use in a PLC Program with user-defined settings.

MLAddReadOff1

Returns the offset value of the first entry of an Adder block.

MLAddReadOff2

Returns the offset value of the second entry of an Adder block.

MLAddReadRatio1

Returns the ratio value of the first entry of an Adder block.

MLAddReadRatio2

Returns the ratio value of the second entry of an Adder block.

MLAddWriteInput

Sets the source of an input of an Adder Pipe Block.

MLAddWriteOff1

Set the offset value of the first entry of the Adder block.

MLAddWriteOff2

Set the offset value of the second entry of the Adder block.

MLAddWriteRat1

Set the ratio value of the first entry of the Adder block.

MLAddWriteRat2

Set the ratio value of the second entry of the Adder block.