MLAxisReadTq

Pipe Network motion icon

 Function - Returns the actual torque applied by the drive mapped to the specified axis.

Inputs

Input

Data Type

Range

Unit

Default

Description

ID

DINT

No range

N/A

No default

Pipe network identifier of the axis block.

Outputs

Output

Data Type

Range

Unit

Description

Torque

LREAL

No range

N.m (Newton meter)

Actual torque applied by the drive associated to the axis.

If the MLAxisRatedTq function is not invoked, the Output value is rated motor continuous torque (where 1000.0 = rated torque).

Remarks

Figure 1: MLAxisReadTq

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

Axis1_Torque := MLAxisReadTq(PipeNetwork.Axis1 )  ;

See Also