MLCNVInit

 Function - Initializes a converter Pipe Block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

-2147483648 to 2147483647

N/A

No default

ID number of a created Pipe Block.

Mode

DINT

1, 2

N/A

No default

Determines the type of input to the Converter Object.

  • 1 for Position mode.
  • 2 for Speed mode.

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Returns TRUE if the Convertor Pipe Block is initialized.

See Function - General Rules.

Remarks

  • MLCNVInit is automatically called if a Convertor Block is added to the Pipe Network, with the input mode (position or speed) entered in the Pipe Blocks Properties screen.
  • The Converter block changes the incoming flow of speed or position values to continuous position output with no periodicity.

  • Converter objects are normally created in the Pipe Network using the graphical engine.
    You do not have to add MLCNVInit function blocks to their programs.
    Parameters are entered directly in pop-up windows and the code is then automatically added to the current project.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

// Initiate a created convertor block named “CNV1”
CNV1 := MLBlkCreate( 'CNV1', 'CONVERTOR' );
MLCNVInit( CNV1, 1 );

See Also