MLBlkCreate

Pipe Network motion icon

 Function - Creates a new Pipe Block object.

Inputs

Input

Data Type

Range

Unit

Default

Description

Name

STRING

No range

N/A

No default

Designated name for the newly created Pipe Block.

Type

STRING

No range

N/A

No default

The type of Pipe Block to create.

Examples: MASTER, GEAR, PHASER, etc.

Outputs

Output

Data Type

Range

Unit

Description

ID

DINT

 

 

Assigned ID number of the created Block.

Remarks

  • Before a Pipe Block is Initialized, the function needs to be created and assigned an ID number.
  • The MLBlkCreate function is automatically called if a Block is added to the Pipe Network.

  • Pipe Blocks are normally created in the Pipe Network using the graphical engine.
    You do not have to add MLBlkCreate function blocks to their programs.
    The code with MLBlkCreate commands are automatically generated and called in a program with Pipe Network(MLPN_CREATE_OBJECTS).

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Create a new  GEAR Pipe Block named “MyGear”
MyGear := MLBlkCreate( 'MyGear', 'GEAR' );

See Also