MLDerInit

Pipe Network motion icon

 Function - Initializes an derivator object.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

-2147483648 to 2147483647

N/A

No default

ID number of a created Pipe Block.

ModuloPosition

LREAL

No range

User units

No default

Input ModuloPosition of Derivator object.

Outputs

Input

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Returns TRUE if the Derivator object is initialized.

See Function - General Rules.

Remarks

  • Function block is automatically called if a Derivator Block is added to the Pipe Network, with user-defined settings entered in the Pipe Blocks Properties screen.
  • Input ModuloPosition is defined to manage the periodicity (modulo) of the input values.

  • Derivator objects are normally created in the Pipe Network using the graphical engine.
    You do not have to add MLDerInit function blocks to their programs.
    Parameters are entered directly in pop-up windows and the code is automatically added to the current project.

Figure 1: MLDerInit

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Create and Initiate a Derivator object 
MyDerivator := MLBlkCreate( 'MyDerivator', 'DERIVATOR' );
MLDerInit( MyDerivator, 360.0 );

See Also