MLGearWriteRatio
Function - Sets the Ratio value of a selected Gear Pipe Block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID number of an initialized Gear Pipe Block. |
|
Ratio |
LREAL |
No range |
User unit/sec |
No default |
New Ratio value to be assigned to the selected Gear Pipe Block.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
No range |
N/A |
Returns TRUE if the Ratio value is changed in the selected Gear Pipe Block. See Function - General Rules. |
Remarks
The output of a Gear Block = Input value * Ratio + Offset.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
//Set the Ratio value of Gear1 Pipe Block to 5
MLGearWriteRatio(PipeNetwork.GEAR1, 5.0);
See Also