MLIntInit

Pipe Network motion icon

 Function - Initializes an integrator object.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

-2147483648 to 2147483647

N/A

No default

ID number of a created Pipe Block.

ModuloPosition

LREAL

No range

User units

No default

Output ModuloPosition of Integrator object.

Modulo

BOOL

FALSE, TRUE

N/A

No default

TRUE when mode is modulo.

Modulo mode adapts the output values according to the ModuloPosition (modulo).

Outputs

Output

Data Type

Range

Unit

Description

Default (.Q)

BOOL

FALSE, TRUE

N/A

Returns TRUE if the Integrator object is initialized.

See Function - General Rules.

Remarks

  • The function block is automatically called if an Integrator Block is added to the Pipe Network.
    • User-defined settings are entered in the Pipe Blocks Properties screen.
  • The Integrator object can operate in modulo or not modulo mode.
    • While in modulo mode, the output values are adapted according to the entered ModuloPosition value.

Figure 1: MLIntInit


  • Integrator objects are normally created in the Pipe Network using the graphical engine.
    You do not have to add MLIntInit function blocks to their programs.
    Parameters are entered directly in pop-up windows.
    The code is automatically added to the current project.

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

//Initiate an Integrator Pipe Block named “MyIntegrator” with a Modulo of 360
MLIntInit(MyIntegrator, 360.0, true );

See Also

MLBlkCreate

MLIntWriteOutVal