MLPhaReadPhase

Pipe Network motion icon

 Function - Gets the phase value of a phaser block.

Inputs

Input

Data Type

Range

Unit

Default

Description

BlockID

DINT

-2147483648 to 2147483647

N/A

No default

ID name of a phaser function block in the Pipe Network.

Outputs

Input

Data Type

Range

Unit

Description

Phase

LREAL

 

 

 

Remarks

None

FBD Language Example

FFLD Language Example

IL Language Example

Not available.

ST Language Example

PresentPhase := MLPhaReadPhase( PipeNetwork.PhaseAdjust );

See Also