acos / acosL

PLCopen motion icon

 Function - Calculate an arc-cosine.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

REAL / LREAL

 

 

 

Real value.

Outputs

Output

Data Type

Range

Unit

Default

Description

Q

REAL / LREAL

 

 

 

Result: Arc-cosine of IN.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.

IL Language Example

  • In the IL Language, the first input must be loaded before the function call.
Op1: LD  IN
     ACOS
     ST  Q    (* Q is: ACOS (IN) *)

ST Language Example

Q := ACOS (IN);

See Also