cos / cosL

PLCopen motion icon

 Function - Calculate a cosine.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

REAL / LREAL

 

 

 

Real value.

Outputs

Output

Data Type

Range

Unit

Description

Q

REAL / LREAL

 

 

Result: Cosine of IN.

Remarks

None

FBD Language Example

FFLD Language Example

  • In the FFLD Language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.

IL Language Example

  • In the IL Language, the input must be loaded in the current result before calling the function.
Op1: LD  IN
     COS
     ST  Q    (* Q is: COS (IN) *)

ST Language Example

Q := COS (IN);

See Also