Create a Program

Once the project has been created and the EtherCAT devices have been defined, a program may be created.

  1. Right-click the Programs item in the project tree and select the language to use.
  2. Name the program.
  3. Click Ok to create the program and open the language-specific editor.

The empty program is ready for you to add functions and function blocks.

Other information you may need to complete your program includes:

See IEC 61131-3 Editors in the Programs: Structure and Syntax section for more in-depth information on the programming languages.