Plug a Probe from the Dictionary
A probe (variable) can be directly plugged or mapped to the Oscilloscope from the Dictionary:
- In the Dictionary, right-click on the variable
- In the menu, select the Map to Oscilloscope channel … command

-
-
This command is enabled if the variable Data Types is eligible for the softscope, as long as they are not in a UDFB instance.
- Define the probe parameters.
There is a difference depending upon whether you selected a Pipe Network probe or a PLC probe.
With Pipe Network variables, select which Data point is being used.
PLC variables may require navigation within the group to find the correct item.

-
-
To enable the Plug on channel… dialog box, the KAS-IDE must be connected to the device first!
Figure 1: Plugging a Probe from the Dictionary
Figure 2: Associating a Pipe Network (left) and PLCopen (right) variable to a Channel.
|
Field |
Description |
|---|---|
|
Channel |
Channel's number where the variable has to be plugged |
|
Data |
Desired variable information to show (the list depends on the type of Pipe Block. See Pipe Block Descriptions for more information. |
|
Derivation Order |
Performs a derivation of the measurement of the selected variable. If this value is different from 0 (zero), the derived value of the selected order is shown on the selected channel. |
|
Derivation Period |
Specifies the modulo period for a periodic variable to remove spikes in the display of derivative orders greater than zero. The value entered should either be 0.0 (No Modulo) or the Modulo Period (e.g., 360.0). |
|
Name |
Variable's name. |
|
Type |
Variable's type. |