Access the Web server From the KAS-IDE

Double-clicking Controller will both expand/collapse the controller's components as well as open the web server and automatically log into the administrator account. For more information on using the webserver see Using the KAS Web server.

The web server can also be accessed by right-clicking the Controller node and selecting Access webserver.


  • IDE users are considered administrators and therefore are automatically logged into the webserver. You may change the password but there is no logout function.

By default the localhost (127.0.0.1) will be opened. To set the IP address of the controller, right click and select Properties. Enter the proper Address and Controller type then click OK. The page is automatically refreshed.

If an invalid or wrong IP address is entered, the following error will be displayed.