Variables tab

The Variables tab is used to show all the variables defined in the project. All the variable details are displayed in order to show the variable types, dimensions, attributes, etc.

Dictionary Toolbox

Figure 1: Variables tab

The list of variables is split into two parts:

Item Number

Description

All the Variables at the top.

All the Structures at the bottom.


  • To show all the variables of all programs, select 'PLC' in the project tree.