AXIS#.PROFINET.​SUPPTELEGRAMID

Description

This parameter is used to select or identify current supplementary data telegram.

If PROFINET.USEMODULECFG = 0, then this command is used to determine which telegram is active.

If PROFINET.USEMODULECFG = 1, then the sub-module/telegram configuration is setup from the PROFINET master and this keyword is blocked.


  • If setting the value for this keyword, the selected telegram data size must be smaller than the telegram configured in the PLC for cyclic data to work correctly.

See AXIS#.PROFINET.​ACTUALVALUEMAP and AXIS#.PROFINET.​SETPOINTMAP

Versions

Action Version Notes
Implemented 02-04-06-000  

General Information

Type Read/Write
Units

N/A

Range N/A
Default Value 970, 971, 972, 973, 5000
Data Type Integer
Stored in Non-Volatile Memory Yes

Variants Supported

PROFINET drives: AKD2G-SPP

Fieldbus Information

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PROFINET.SUPPTELEGRAMID

5212

Unsigned16

Read Only

-