AXIS#.VL.KFB
Description
AXIS#.VL.KFB allows the user to scale the velocity feedback source into the velocity control loops
This is especially useful in dual-loop applications where the position loop feedback and velocity loop feedback come from different devices. AXIS#.PL.KFB and AXIS#.VL.KFB can be used to synchronize the values.
Examples
Usage
By default AXIS#.VL.KFB is set to 1.0 and should not be set to another value unless the application is using multiple feedback devices for a axis.
If the situation arose where two feedbacks were mounted to a rotary motor, and one of them was half the resolution of the first - and it was connected to the position feedback, while the full resolution device was connected to the velocity feedback, AXIS#.PL.KFB would need to be set to 2.0 and AXIS#.VL.KFB would be left at 1.0.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | Double |
| Default Value | 1 |
| Data Type | Float |
| See Also | AXIS#.PL.KFB |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
Supported on all device types.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.VL.KFB |
5011h |
23h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.VL.KFB |
5111h |
23h |
Signed32 |
- |
1000:1 |
Read/Write |
No |