REC.ACTIVE

Description

REC.ACTIVE indicates whether or not data recording is in progress. Recording is in progress if the trigger was met and the recorder is recording all data.

Examples

Code

Indicates that recording is not in progress.

-->REC.ACTIVE
0

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

N/A

Data Type

Integer

See Also

REC.DONE , REC.OFF

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REC.ACTIVE

2300

8FC

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REC.ACTIVE

2300

Unsigned8

Read Only

-