REC.OFF
Description
REC.OFF turns the recorder off. In order to set the recorder again, the recorder must first be armed and then a trigger set.
Examples
Code
If a recording is triggered before this command is executed, this command will cancel the recording and the recording state will go to Idle.
-->REC.OFF
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
REC.OFF |
2304 |
900 |
Unsigned8 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REC.OFF |
2304 |
Unsigned8 |
Read/Write |
- |