REC.TRIG

Description

REC.TRIG starts the trigger according to the trigger type defined by REC.TRIGTYPE.

REC.TRIG sets the value of REC.DONE to 0.

After calling REC.TRIG, the data that was recorded by previous recording is deleted and cannot be retrieved.

No REC parameters can be set after a call to REC.TRIG until the recorder has finished or until REC.OFF is executed.

Example

Code

If a trigger is set up, this command will arm the trigger. If the recording is "Immediate", this command will start the recording.

-->REC.TRIG

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

REC.RETRIEVE, REC.OFF

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

REC.TRIG

2306

902

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

REC.TRIG

2306

Unsigned8

Read/Write

-