AXIS#.SAFEPARAM.SBC​.MUTINGSOURCE

Description

This parameter allows the user to specify a safe input to bypass Safe Brake Control (SBC) and permit the brake to release regardless of whether SBC is active or not. The feature is referred to as ‘SBC Muting’ in documentation and WorkBench.

Value Description

0

Not used

1

Safe input 1

2

Safe input 2

3

Safe input 3

4

Safe input 4

5

Safe dual input 1

6

Safe dual input 2

If using this feature, make sure it is safe to release the brake and there is not a heavy load being held solely by the brake.

Parameters Editor with the SBC Muting value of Not Used circled

Context

For complete SBC information refer to SBC (Safe Brake Control).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-01-02-000

General Information

Type

Read/Write

Units

N/A

Range

0 or 6

Default Value

N/A

Data Type

Integer

Stored in Non- Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SBC.MUTINGSOURCE

3156h

04h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SBC.MUTINGSOURCE

3256h

04h

Unsigned8

-

-

Read/Write

No