DIN.STATES
Description
DIN.STATES reads the states of the digital inputs.
-
-
AKD-N only supports DIN1 to DIN3.
-
-
AKD-N only supports DIN1 to DIN2.
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
0000000 to 1111111 |
Default Value |
N/A |
Data Type |
String |
Start Version |
M_01-00-00-000 |
AKD-N Information | |
---|---|
Range | 000 to 111 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | Yes |