IL.LIMITN

Description

This parameter sets the negative user limit clamp value of the torque-producing q-component current command (IL.CMD). The current command is additionally limited by the motor peak current setting (MOTOR.IPEAK) and by the present value of the foldback I²t peak motor current protection.


  • This current limit is overwritten by MT.FIXEDSTOPCURRENT while a fixed stop motion task is running in a negative direction. Once the motion task is complete, the limit is restored to the previous IL.LIMITN value.

General Information

Type

NV Parameter

Units

A

Range

Negative drive peak current (DRV.IPEAK) to 0 A

Default Value

Negative drive peak current (DRV.IPEAK)

Data Type

Float

See Also

IL.LIMITP

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
356Fh/0 M_01-00-00-000

Related Topics

"Current Loop"