IL.OFFSET
Description
This value is added to the overall current loop feedforward value.
General Information
|
Type |
RW Parameter |
|
Units |
A |
|
Range |
|
|
Default Value |
0 A |
|
Data Type |
Float |
|
See Also |
IL.FF |
|
Start Version |
M_01-00-00-000 |
| Variant | Supported |
|---|---|
| MKD EtherCAT | Yes |
| AKD-N | Yes |
| MKD-N | Yes |
| MKD-C | No |
| Index/Subindex | Object Start Version |
|---|---|
| 3423h/0 | M_01-00-00-000 |
Related Topics