PipeNetwork_FFLD - Special FFLD Function
Function - Calls the PNCode function block in FFLD POUs.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
En |
BOOL |
0 to 1 |
N/A |
No default |
Request to initialize the Pipe Network. |
|
cmdID |
DINT |
N/A |
N/A |
No default |
Commands used to start and initialize the Pipe Network.
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
OK |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. |
Remarks
- It starts and initializes the Pipe Network, based on the command specified by cmdID.
- Internally this function calls the Function Block PNCode.
- This is a special function.
- It should only be used in Pipe Network applications that contain FFLD POUs that call PNCode.
- To use this function, Pipe Network must be declared as a global variable in the dictionary.
- Calling this function instead of PNCode in FFLD POUs eliminates this compile error that occurs after modifying the Pipe Network using the Pipe Network editor:
Controller:PLC:Main: NW1(1,14): PNCode: Invalid block height
- The compile error is generated because the number of outputs on PNCode can vary.
- This occurs after modifying the original Pipe Network using the Pipe Network editor.
- The new PNCode Function Block is not automatically updated in any FFLD POUs, reflecting the new outputs.
- Manually update each PNCode function block call in any FFLD POUs to correct this problem.
-
-
The Pipe Network FFLD Application Template is a good example of how to use this Function.
See Pipe Network 2-Axes Template - FFLD.
Figure 1: PipeNetwork_FFLD
FBD Language Example
Not available.
FFLD Language Example
IL Language Example
Not available.
ST Language Example
Not available.
See Also