MLAxisRatedTq
Function - Allows conversion of drive torque values from rated torque units
(1000 = rated motor continuous torque) to N.m (Newton meter).
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
ID |
DINT |
No range |
N/A |
No default |
Pipe network identifier of the axis block. |
|
Torque |
LREAL |
No range |
N.m (Newton meter) |
|
Actual torque applied by the drive associated to the axis. Rated torque = Nominal Drive Current * Torque factor = DRV.ICONT * MOTOR.KT. DRV.ICONT is obtained by SDO parameter: index 5083h (sub-index 0). MOTOR.KT is obtained by SDO parameter: index 3593h (sub-index 0). See:
To read/write an SDO object with an index greater than 16#7FFF (32767), the value must be entered in this form: Example:
|
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. See Function - General Rules. |
Remarks
Figure 1: MLAxisRatedTq
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLAxisRatedTq(PipeNetwork.Axis1, Axis1_Torque ) ;
See Also