MLMstWriteSpeed
Function - Sets the speed of a master block.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
EN |
BOOL |
FALSE, TRUE |
N/A |
No default |
Enables the FB to be executed. |
|
BlockID |
DINT |
-2147483648 to 2147483647 |
N/A |
No default |
ID name of the Master Block. |
|
Speed |
LREAL |
No range |
User unit/sec |
No default |
Speed of the motion. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Default (.Q) |
BOOL |
FALSE, TRUE |
N/A |
Returns TRUE when the function successfully executes. See Function - General Rules. |
Remarks
- Set the speed of motion for the MLMstAbs and MLMstRel blocks.
- This function or function block does not generate any motion.
FBD Language Example
FFLD Language Example
IL Language Example
Not available.
ST Language Example
MLMstWriteSpeed( PipeNetwork.MASTER, 400.0 );
See Also