max
Function - Get the maximum of two integers.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN1 |
ANY |
|
|
|
First input. |
|
IN2 |
ANY |
|
|
|
Second input. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
ANY |
|
|
IN1 if IN1 > IN2; IN2 otherwise. |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables the operation.
- The output rung keeps the state of the input rung.
- The comparison is executed only if EN is TRUE.
- ENO has the same value as EN.
IL Language Example
- In the IL Language, the first input must be loaded before the function call.
- The second input is the operand of the function.
Op1: LD IN1
MAX IN2
ST Q (* Q is the maximum of IN1 and IN2 *)
ST Language Example
Q := MAX (IN1, IN2);
See Also