mod / modLR / modR
Function - Calculation of modulo.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
IN |
mod = DINT modR = REAL modLR = LREAL |
|
|
|
Input value. |
|
BASE |
mod = DINT modR = REAL modLR = LREAL |
|
|
|
Base of the modulo. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Q |
mod = DINT modR = REAL modLR = LREAL |
|
|
Modulo: rest of the integer division (IN / BASE). |
Remarks
None
FBD Language Example
FFLD Language Example
- In the FFLD Language, the input rung (EN) enables the operation.
- The output rung keeps the state of the input rung.
- The comparison is executed only if EN is TRUE.
- ENO has the same value as EN.
IL Language Example
- In the IL Language, the first input must be loaded before the function call.
- The second input is the operand of the function.
Op1: LD IN
MOD BASE
ST Q (* Q is the rest of integer division: IN / BASE *)
ST Language Example
Q := MOD (IN, BASE);
See Also