Compiler Errors
These errors may be seen when compiling a project.
![Closed](../../Skins/Default/Stylesheets/Images/transparent.gif)
"EtherCAT: ERROR: Failed to retrieve EtherCAT device…"
These errors indicate either:
- The ESI file for the EtherCAT device is missing.
- Information is missing from the ESI file for a device and/or module.
Examples
EtherCAT: ------------- Generating EtherCAT Network Information (ENI) file ---------------
EtherCAT: ERROR: Failed to retrieve Vendor for vendorID=0x21 in ESI cache
Project compile failed
EtherCAT: ------------- Generating EtherCAT Network Information (ENI) file ---------------
EtherCAT: ERROR: Failed to retrieve EtherCAT device (vendorID=0x2, productCode=0x44c2c52, revision=0x120000) in ESI cache
Project compile failed
Error Correction
- Identify which EtherCAT devices or modules are listed as Unknown in the Project View.
- Import an appropriate ESI file.
See Unknown – Missing ESI File for more information.
![Closed](../../Skins/Default/Stylesheets/Images/transparent.gif)
"Failed to export ENI file, check the logs for more details." or
"EtherCAT: Warning : In AKD_1, PDO object index 0x3470, subIndex 4 is redundant."
These errors indicate redundant PDO entries.
Error Correction
See Redundant PDO Entries for more information.
![Closed](../../Skins/Default/Stylesheets/Images/transparent.gif)
These compiler outputs indicate a failure to compile the optimized C code:
Controller:PLC:> ------------- Compile Optimized Code -------------
Controller:PLC:> Compiling "C" code.
Controller:PLC:> ERROR: Failed to compile PLC "C" code.
Controller:PLC:> Compilation log:
...
Controller:PLC:> End of Compilation log
Controller:PLC:> Compile Time Elapsed:1.37 seconds
Controller:PLC:> ------------- Compile Optimized Code FAILED -------------
Error Correction
Locate and send these items to Kollmorgen technical support:
- The compilation log (copied from the compiler output).
- All the files in this directory:
%LOCALAPPDATA%\Kollmorgen\KAS\Project\Controller\PLC\CC\
- The path can be copied and pasted into the Windows Explorer address bar.
To help us resolve the error with you, Kollmorgen technical support contact information can be found here:
Call or e-mail the appropriate support for your region.
![Closed](../../Skins/Default/Stylesheets/Images/transparent.gif)
A possible cause for optimized PLC code to fail compilation is if the user does not have permission to write to an output file or folder.
Example 1: The file cclog.txt is not writeable.
Controller:PLC:> ------------- Compile Optimized Code -------------
Controller:PLC:> ERROR: cannot remove old output file "C:\Users\my.name\AppData\Local\Kollmorgen\KAS\Project\Controller\PLC\CC\cclog.txt"
Controller:PLC: > To resolve the issue, set the permissions on the file so that it is writeable.
Controller:PLC:> Compile Time Elapsed:0.02 seconds
Controller:PLC:> ------------- Compile Optimized Code FAILED -------------
Example 2: The file main.c is not writeable.
Controller:------------- Compile PLC ---------------
...
Controller:PLC:main
Controller:PLC:c:\users\my.name\appdata\local\kollmorgen\kas\project\controller\plc\cc\main.c:
Cant write output file
Controller:PLC:appli
Controller:PLC:Error(s) detected
Controller:------------- PLC failed ---------------
Error Correction
Change the file permissions to allow writing to the file.
![Closed](../../Skins/Default/Stylesheets/Images/transparent.gif)
"Boolean expression expected after IF."
These errors indicate that the IF THEN ELSE ELSIF END_IF condition used in the application code does not evaluate to a BOOL expression.
Controller:------------- Compile PLC ---------------
…
Controller:PLC:MCFB_Jog
Controller:PLC:MCFB_Jog: (16): Unexpected complex data in expression
Controller:PLC:MCFB_Jog: (16): Boolean expression expected after IF
Controller:PLC:MCFB_Jog: (19): END_IF: New statement expected
Controller:PLC:Error(s) detected
Controller:------------- PLC failed ---------------
Controller:------------- Device compile failed ---------------
...
Project compile failed
This compile error can happen when a non-compliant syntax is used for verifying the function block outputs.
- In the KAS v4.0 and earlier releases, it was possible to use the function block return statement in the same way as function return values.
- This could result in undefined behavior.
- In KAS v4.0 and later releases, the compiler generates a an Unexpected complex data in expression error for non-compliant syntax.
IEC 61131-3 Non-Compliant Syntax:
If inst_functionBlock(myVar1) Then
// ...
End_If;IEC 61131-3 Compliant Syntax:
inst_functionBlock(myVar1);
If inst_functionBlock.Q Then
// ...
End_If;
Error Correction
- Identify the code that caused compile error.
- If the error is due to non-compliant syntax, replace this code using compliant syntax for the corresponding function block.
Example: Non-compliant Syntax
IF Inst_r_trig(Inst_TON.Q) THEN
Inst_DriveParamRead( TRUE, any_to_int(Inst_MC_ReadParam.Value), 'DRV.FAULT1' );
END_IF;
Example: Compliant Syntax
Inst_r_trig(Inst_TON.Q);
IF Inst_r_trig.Q THEN
Inst_DriveParamRead( TRUE, any_to_int(Inst_MC_ReadParam.Value), 'DRV.FAULT1' );
END_IF;
-
- UDFBs and libraries can have improper syntax.
These Kollmorgen UDFBs have been corrected and can be re-imported into the application code.
See Re-import Kollmorgen UDFBs for more information.