Resume Camming After an E-Stop
The MC_CamResumePos function block is used to return a slave axis to its profile position after an event (such as an E-stop) caused the slave axis to go off path.
To return a slave axis to its MC_CamIn profile position, the typical programming sequence is:
- With the master axis at standstill, call MC_CamResumePos to determine the profile position for the slave axis.
- Call MC_MoveAbsolute to move the slave axis to the position calculated by MC_CamResumePos.
- Call MC_CamIn with
StartMode = 1(Resume mode).