Configure EtherCAT Motion Bus
-
-
Before configuring the EtherCAT settings, you may want to add third party EtherCAT devices.
See Add and Configure Third Party EtherCAT Devices for more information.
This window has these tabs:
|
Tab |
Description |
|---|---|
|
Displays all the E-Bus devices present in the project tree. |
|
|
Used to configure the EtherCAT bus master. |
|
|
Used for an external configuration file. |
|
|
Display, add, and remove available ESI files. |
KAS includes an integrated tool to configure the EtherCAT master and start up the fieldbus operation.
Use the configuration tool to:
- Describe your motion Topology as a configuration tree.
- See the procedure in EtherCAT Devices tab.
- Associate variables to the I/O channels of devices.
- See the procedure in Map Input and Output to Variables.
Slave Devices
Slave devices can support several PDOs.
-
-
PDOs contain real-time cyclic data which is deterministic.
Non-cyclic data is not deterministic and is defined by Service Data Objects (ScDO).
In EtherCAT Motion Bus Concepts, input and output parameters are grouped in predefined blocks called PDOs.
- Some PDOs are mandatory; others are optional.
- See click here... for the list.
- One of the main tasks of the EtherCAT configuration is to select the PDOs used by each slave and group them all in the EtherCAT image.
- See EtherCAT Devices Summary Form for more information.