Boot Sequence
-
-
The controller may be booted with or without an Ethernet cable attached.
These are the controller boot sequences:
When the controller is booted with a cable attached, the configured IP address (depending upon the current position of the rotary switch) appears in the 7-segment display.
- See View the Controller IP Address for more information.
- If the controller is started without a network connection then the IP address is not displayed.
- After the boot sequence is successful, the controller is in one of two modes:
|
|
Normal operation. |
|
|
Recovery Mode (if firmware download is permitted). |
AKD PDMM or PCMM Boot Sequence
This is the boot sequence for either the AKD PDMM or PCMM:
|
State |
Display |
Description |
|---|---|---|
|
Hardware Power ON |
|
The controller option card has power. |
|
Stage 0 |
|
This is reached after the I2C is initialized. |
|
Stage 1 |
|
This is reached after the DDR3 ram memory is initialized. |
|
Stage 2 |
|
This is reached just after the RAM memory relocation. |
|
Stage 3 |
|
Reached after the flash memory is initialized. |
|
|
After all the previous steps, the startup script starts automatically. |
|
|
QNX startup |
|
This is reached after the Boot startup script is finished. |
|
Sysinit |
|
This is reached after:
|
PCMM2G Boot Sequence
These are the boot sequences of the PCMM2G:
Internal Flash
-
- If the controller is stuck in Stages 1 to 4, then recovery could be made by using the
B3 button to boot off of the inactive partition.
See Boot from Inactive Partition Image - PCMM2G.
|
State |
Display |
Description |
|---|---|---|
|
Hardware Power ON |
|
PCMM2G has power. |
|
Stage 1 |
|
Bootloader completed. Starting U-Boot. |
|
Stage 2 |
|
U-Boot succeeded. Starting Linux Kernel. |
|
Stage 3 |
|
Linux Kernel is up. PCMM2G processes Initializing. |
|
Stage 4 |
|
Starting:
|
|
Final Stage |
|
Runtime started. |
Recovery USB Drive
See PCMM2G Web server Recovery.
-
- If the controller is stuck in Stages 1 to 4, then recovery could be made by using the
B2 button to boot off of the recovery USB drive.
See Boot from Recovery Image (B2 Button).
|
State |
Display |
Description |
|---|---|---|
|
Hardware Power ON |
|
PCMM2G has power. |
|
Stage 1 |
|
Starting U-Boot from recovery USB drive. |
|
Stage 2 |
|
U-Boot succeeded. Starting Linux Kernel. |
|
Stage 3 |
|
Linux Kernel is up. PCMM2G processes Initializing. |
|
Stage 4 |
|
Starting:
|
|
Final Stage |
|
Recovery runtime started. |