|
Online Configuration Mode
|
This action is only available when the KAS Runtime is connected with the target Controller.
- Click this toggle button to change the mode (ON / OFF).
- After the scan has been performed, and your project is compliant with the physical devices on the EtherCAT network, you can activate the Online Configuration Mode.
- Online Configuration Mode allows setting up AKD and AKD2G drives in an EtherCAT installation.
- In this mode, KAS-IDE communicates with the drives through the integrated views of the AKD Setup Screens or with the AKD Setup Wizard.
- KAS-IDE displays a quick status overview of all the drives.
- The AKD Setup Screens allow functions (e.g., enabling / disabling the drive, service motion, tuning, and a scope) where you can plot up to six different parameters from the drive.
- See click here... for more details on the AKD Setup screens.
- See click here... for more information.
- See FAQs for a potential issue when resetting the factory parameters.
|