AXIS#.MOTOR.NAME
Description
This parameter is the motor name.
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
20 chars |
|
Default Value |
empty |
|
Data Type |
String |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6237 |
1 |
6237 (0x185d) |
AXIS1.MOTOR.NAME |
String |
Read Only |
No |
|
71773 |
2 |
6237 (0x185d) |
AXIS2.MOTOR.NAME |
String |
Read Only |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.NAME |
6237 |
String |
Read Only |
- |