DRV.DISSOURCES

Description

DRV.DISSOURCES is a bitwise parameter that returns the status of possible causes of a drive disable. If this parameter is 0, then the drive is enabled.

The return value specific bits are as follows:

Bit

Status and Response

Drive Action

0

Software disable (execute DRV.EN to issue software enable)

Performs action configured by DRV.DISMODE.

1

Fault exists (read DRV.FAULTS to get the active faults)

Device disables using the defined reaction for the detected fault.

2

Hardware disable (remote enable input is low)

Power stage disabled.

3

In-rush disable (the in-rush relay is opened)

Performs action configured by DRV.DISMODE.

4

Initialization disable (the drive did not finish the initialization process)

Power stage disabled.

5

Controlled stop disable from a digital input.

Controlled stop.
6 Field Bus requested disable (SynqNet and EtherNet/IP only) Performs action configured by DRV.DISMODE.
7 AKD-C requested disable (AKD-N only) Performs action configured by DRV.DISMODE.
8 AKD pre-charge disable (AKD-C only). Discharge strings voltage.
10 AKD-C in download mode. Disables all AKD-Ns on the AKD-C's strings.

The states indicated by this keyword, can be viewed by clicking the "Axis active/Axis inactive" button at the bottom of WorkBench:

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3443h/0

M_01-00-00-000

Related Topics

Controlled Stop

DRV.ACTIVE, DRV.FAULTS, DRV.EN, DRV.DIS