DRV.EN

Description

DRV.EN issues a software enable to the drive. You can query the value of DRV.ACTIVE to check whether the drive is currently enabled or disabled.

You can also query the value of DRV.DISSOURCES to check whether the software enable bit is high (software enabled was issued by executing DRV.EN) or the software enable bit is low (software disable was issued by executing DRV.DIS). If the drive software enable bit is low and DRV.EN is executed, then drive faults are automatically cleared during the software enable process.

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

Analog drive software is enabled.

All other types of drive software are disabled.

Data Type

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No

*For PROFINET, write a value of 0 into the PNU to execute a command.

Related Topics

"Clearing Faults"

"Enable/Disable"

DRV.DIS, DRV.DISSOURCES,DRV.ACTIVE