MOTOR.BRAKE

Description

The MOTOR.BRAKE parameter notifies the firmware whether a brake exists or not. It does not apply or release the brake. If a brake is found to be present, the firmware considers hardware indications regarding the brake circuits (such as open circuit or short circuit). If a brake does not exist, then the firmware ignores the hardware indications since they are irrelevant.

Value Status

0

Motor brake does not exist.

1

Motor brake exists and brake hardware circuitry checks are enabled.

100 For special, low current, brake applications, the F305 fault can be bypassed with this setting.

Enabling the MOTOR.BRAKE (value set to 1) when no motor brake exists creates a fault.

The motor brake is polled every 16ms.

General Information

Type

NV Parameter

Units

N/A

Range

0, 1, 100

Default Value

0

Data Type

Boolean

See Also

N/A

Start Version

M_01-00-00-000

AKD BASIC Information
Data Type Integer
Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version
3587h/0 M_01-00-00-000

Related Topics

"Motor View"