MOTOR.ICONT
Description
This parameter is used to configure the motor continuous current.
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
General Information
Type |
NV Parameter |
Units |
A |
Range |
0.1 to 500 A |
Default Value |
1.0 A |
Data Type |
Float |
See Also |
N/A |
Start Version |
M_01-00-00-000 |
AKD BASIC Information |
|
---|---|
Type |
R/W |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | No |
Index/Subindex | Object Start Version |
---|---|
358Eh/0 | M_01-00-00-000 |
Related Topics