MOTOR.NAME
Description
This parameter is used to set the motor name.
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
20 chars |
Default Value |
N/A |
Data Type |
String |
See Also |
N/A |
Start Version |
M_01-00-00-000 |
Variant | Supported |
---|---|
MKD EtherCAT | Yes |
AKD-N | Yes |
MKD-N | Yes |
MKD-C | No |
Index/Subindex | Object Start Version |
---|---|
3899h/0 | M_01-19-04-000 |
Related Topics