MOTOR.TEMP

Description

This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.

General Information

Type

R/O Parameter

Units

Range

0 to 232

Default Value

N/A

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCAT Yes
AKD-N Yes
MKD-N Yes
MKD-C No
EtherCAT CoE and CANopen
Index/Subindex Object Start Version

3612h/0

M_01-00-00-000

Related Topics

Motor View | MOTOR.RTYPE